Other Parts Discussed in Thread: TLV320ADC6140, TLV320ADC3140, TLV320ADC5140
I need to implement a digital filter after amplifier opa1654 circuit, do you have a sugestion what DSP component can I use?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to implement a digital filter after amplifier opa1654 circuit, do you have a sugestion what DSP component can I use?
Hello Airton,
From the basic description you have given here, my first estimate is that you will likely need an ADC that can handle 4 inputs along with digital filtering, such as TLV320ADC6140. I'm going to move this post into the ADC forum.
Best Regards,
Mike
Good morning Carson!
I receive a senoidal signal , between 5 a 15 Khz, and I need analyze the amplitude and fase variation, removing noise, I need improve de signal gain and reject noise.
So where is the digital signal coming from? or do you need to convert to digital then filter then reconvert to analog?
I need to convert to digital, filter and analyze the result, meassure the variations of fase and amplitude of the signal.
Hello,
Let me browse for a device that could suite these needs and I will reply back in 48 hours.
Best Regards,
Carson
Hello,
Best options here are TLV320ADC3140, TLV320ADC5140, or TLV320ADC6140 with them all being same except SNR improves as the first digit goes from 3 to 5 to 6. They have most filtering capability of our ADCs.
Best Regards,
Carson