Hello,
As part of my design, we have 3 biquad filters where the coefficients were calculated based on a 32kHz sampling rate.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
As part of my design, we have 3 biquad filters where the coefficients were calculated based on a 32kHz sampling rate.
Hello Santhosh,
Yes, you can use the same coefficients but the filter cut-off frequency will scale with the sampling rate. For example, if you have a lowpass filter with roll-off at 2kHz that is calculated for a 16kHz sampling rate.. when the sample rate is changed to 8kHz the roll-off will scale down to 1kHz.