This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1681: Customer wants to combined use LRCK for DSD compatible model

Part Number: PCM1681
Other Parts Discussed in Thread: PCM9211, PCM1862,

Hello expert,

This is Koki Tsushima.

I want to ask about PCM1681 can be used LRCK for DSD compatible model.

Customer wants to common I2S between this PCM1681 and other DAC.

When the situation above on DSD, are there no issues to input the DSD data to PCM1681?

For that time, LRCK will be DSD and DSD can be 2.8M to 11.2MHz.

I know PCM1681 is not for DSD DAC, but I want to ask it is possible to combined use LRCK.

Best regards,

Koki Tsushima