Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DIX9211: About RXIN"0" input of DIX9211.

Part Number: DIX9211

Hello.
We are considering a configuration in which Buffer is added to the front and "SPDIF input→Buffer→DIX9211".
Is it okay to connect the CMOS output directly to RXIN0 of DIX9211?

Thanks.
Regards.

  • Hello,

    Input impedance is 20 kohms and they internally tied high if inputs are not powered on. This device was not made with a CMOS input in mind but for coaxial but based from here in datasheet it seems like it would be okay.

    Best Regards,

    Carson