Part Number: PCM5121
Hi team,
My customer use PCM5121 in their project, now they meet below issue, could you help give some suggestions? Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM5121
Hi team,
My customer use PCM5121 in their project, now they meet below issue, could you help give some suggestions? Thank you!
Hi Ivy, let me take a look at the schematic and issue and will reply to you by the end of the week.
Regards,
Arash
Hi Ivy,
From schematic review I have few suggestions: put more caps on LDO pin, also from connections of MODE2 and MODE1 , pin 10 is VCOM, which needs do be connected to GND via a decoupling cap ( Datasheet: VCOM output (optional mode selected by register; default setting is VREF mode.) When in VREF mode (default), this pin ties to GND. When in VCOM mode, decoupling capacitor to GND is required.
So while they play a signal, with fs=48, at some time the clk halts and thus parts go to standby mode , then at this time they change to fs=96k and they hear a pop. Can you clarify that clk is running and part is out of standby ? I am not able to see the complete steps and procedure. Can you please elaborate the sequence in more details?
Thanks,
Arash
Hi Arash,
Thanks a lot for your suggestions!
1. For the number of caps and the capacity value to be added, could you please help to give some suggestions?
2.
=》PCM5121 I2S slave mode
Thanks!
Regards,
Ivy
Hello Ivy,
for various cap sizes they can refer to User's Guide SLAU444A, if there is no info for a cap put a 2.2uF for decupling.
Did you ask them to correct VCOM connection and see if it makes any difference?
Regards,
Arash