This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA2050D4 gain question

Other Parts Discussed in Thread: TPA2054D4, TPA2050D4

Dear Sir,

I have check the TPA2054D4 datasheet, it is pin to pin with TPA2050D4.
TPA2054D4 have +6dB before PWM, is TPA2050D4 the same ?

  • Hello iehncent,

    The TPA2054D4 and TPA2050D4 are not quite pin to pin compatible.  The TPA2054D4 has an extra Mono differential input.  Also, the TPA2054D4 has a Class-D gain of +6 dB, whereas in the case of the TPA2050D4 it's 0 dB.

    Please see attached diagram showing pinout differences.

    Best regards,

    Alfredo Barriga

    Audio applications engineer

    Dallas, TX - USA

     

    8867.TPA2054_Vs_TPA2050.pdf