In the datasheet, it said TPD3118D2 can support 2x 30W@8ohm, 24V. How about 2x15W (stereo) and 1x 30W (woofer) @4ohm, 12V?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the datasheet, it said TPD3118D2 can support 2x 30W@8ohm, 24V. How about 2x15W (stereo) and 1x 30W (woofer) @4ohm, 12V?
Thanks
Hi Jacky
It's not so related to efficiency because we can increase the current when efficiency is low.
The Rdson of MOSFET and inductor will divide voltage from load. We usually assume a -0.5dB voltage will lost on these devices. So with 12V PVDD, the max voltage on load is around 11.3V. The output on load is always sine wave, you need to use the RMS value to calculate power. It's 11.3^2 / 2 / 4 = 15.96W.
For stereo 4ohm, 12V --> the max output power is 15.96W and the current would be 1.14A at each channel, can the TPA3118D2 sustain the heat at 60C ambient temperature? if not, what is the max power can be supported for stereo 4ohm, 12V at 60C?
Hi Jacky
We think there should be no problem to produce 15.96W. You can use more vias and copper on the PCB to help dissipate heat, and the heat sink can be considered.