Other Parts Discussed in Thread: NE5534, PCM1794
Hi,TI !
I used the external filter mode for digital-to-analog conversion,and I used the IOUTL differential pair outputs in the circuit diagram using the NE5534 in the datasheet.
Are the following Settings appropriate for PCM1794?
Settings:
BCK 25Mhz
DATA 24-bit
WDCK 1Mhz
SCK 24Mhz or 50Mhz
I used these Settings because I need to feed DATA into PCM1794 in a us. When I used these Settings ,the output of NE5534 is always -5.8V. No matter what the DATA is, the output is always -6.3V.
Thanks for any help in this.
tq