This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV135: Two drivers with their outputs tied together

Part Number: DRV135

If I'm using two DRV135 audio drivers and the outputs of both drivers are tied together, will this cause damage to the one of the drivers when the other one has a stimulus applied to it?  Will this cause the second drivers output to be driven if the first driver is powered on or are there safety measures on the chips to prevent this?