This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3204: Configuration - HPL, HPR, LOL and LOR Routing Selection Registers

Part Number: TLV320AIC3204

Hello,

We are using TLV320AIC3204 in our products and I need to make some changes to the ALSA driver. We need to use both HP and LO outputs simultaneously. So we are planning to use Left DAC for HP outputs and Right DAC for LO outputs as described in Figure 2-4 and Figure 2-9 in SLAA557–November 2012 edition document.

So for the HP output configuration (using Left DAC), I can enable Page 1 Register 12 D3 (Left DAC+) and Register 13 D4(Left DAC-) bits to get the above configuration. 
But for LO configuration (using Right DAC)

  1. Should I enable Page 1 Register 14 D4 (Right DAC-) and Page 1 Register 15 D3(Right DAC)? For register 15 D3 doesn't specify whether it is +ve or -ve from Right DAC.
  2. Or should I enable Page 1 Register 14 D0 and Page 1 Register 15 D3? 

Also, Register 14 D3 doesn't specify whether it is +ve or -ve from the DAC.

Thanks

Santosh