Hi expert,
I want to ask three questions for PCM1681.
Q1
How should be un-used pin for DATA1-4? Is it OK to be Open or needs to be connected to pull-down resistors? If the later, could you tell me the recommended values of pull-down resistor?
Q2
Let me confirm to make sure when the case which Glitch noise (=short pulse than normal "high" signal) is input to SCK/ BCK /LRCK.
For that time, will not be hung if Glitch noise for 1 pulse is input to them when SCK/ BCK /LRCK was inputted or loss?
I personally think this is yes, by refer to former E2E by me
If an unexpected DSD data signal is sent to LRCK, no damage will be resulted, because as far as the pin is concerned, just a "wrong" signal is sent to it and therefore the part should not function.
Is this understanding correct?
Q3
Let me confirm to make sure when DSD data may be also input.
it may be hung for worst scenario if DSD data was inputted to LRCK of PCM1681.
Therefore, customer try to keep "L" for LRCK when DSD audio was played by changing their circuit.
Is this solution a good way to solve the hung for worst scenario?
Customer think that there are no issue if DSD data was inputted to SCK/BCK because the frequency for DSD and PCM are same (i.e. DSD 2.8M → 22.57MHz/2.82Mz).
If this is true, though there is DSD data for DATA pin, but goes into suspend and the data will be ignored, then the music will be played again when all CLK was correct and synchronized.
Are those thinking true?
Best regards,
Koki Tsushima