This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5252: Designing a 2 DAC system for a 3 way speaker

Part Number: PCM5252
Other Parts Discussed in Thread: TPA3251,

Hi There,

I am designing a 3 way speaker which will be connected to a TPA3251 amplifier, set up in a 2 x Single Ended + 1 x BTL mode. To do this I require 3 DAC channels Treble, mid range and bass. After reviewing the PCM5252 architecture it looks like it is feasible to connect multiple PCM 5252 chips together and I note there are already some products available that do this. Do you have a reference architecture that shows how to do this? I will be using an I2S connection to the primary PCM5252. I am not sure if we want to use the clock on the PCM chip or not. 

Thanks in advance

Iain