Hi,
I want to use the on-board microphone of the tlv320aic3254evm-k card and I'm looking for the configuration to be able to use it with my processing chain and get the sound from the output of the card (without the bypass).
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to use the on-board microphone of the tlv320aic3254evm-k card and I'm looking for the configuration to be able to use it with my processing chain and get the sound from the output of the card (without the bypass).
Best regards,
Hi,
You can start with the attached configuration file.
############################################### # On-Board Differential Microphone # --------------------------------------------- # PowerTune mode PTM_R4 is used for high # performance 16-bit audio. # # For normal USB Audio, no hardware change # is required. # # If using an external interface, SW2.4 and # SW2.5 of the USB-ModEVM must be set to # HI and clocks can be connected to J14 of # the USB-ModEVM. # # IN3L/R is are routed differentially to the # LADC. ############################################### ############################################### # Software Reset ############################################### # # Select Page 0 w 30 00 00 # # Initialize the device through software reset w 30 01 01 # ############################################### ############################################### # Clock Settings # --------------------------------------------- # The codec receives: MCLK = 11.2896 MHz, # BLCK = 2.8224 MHz, WCLK = 44.1 kHz ############################################### # # Select Page 0 w 30 00 00 # # NADC = 1, MADC = 2 w 30 12 81 82 # ############################################### ############################################### # Signal Processing Settings ############################################### # # Select Page 0 w 30 00 00 # # Set the ADC Mode to PRB_P1 w 30 3d 01 # ############################################### ############################################### # Initialize Codec ############################################### # # Select Page 1 w 30 00 01 # # Disable weak AVDD in presence of external # AVDD supply w 30 01 08 # # Enable Master Analog Power Control w 30 02 00 # # Select ADC PTM_R4 w 30 3d 00 # # Set the input powerup time to 3.1ms (for ADC) w 30 47 32 # # Set the REF charging time to 40ms w 30 7b 01 # ############################################### ############################################### # Recording Setup ############################################### # # Select Page 1 w 30 00 01 # # Powerup MIC BIAS w 30 33 40 # # Route IN3L to LEFT_P with 10K input impedance w 30 34 04 # # Route IN3R to LEFT_M with 10K input impedance w 30 36 04 # # Unmute Left MICPGA w 30 3b 00 # # Unmute Right MICPGA w 30 3c 00 # # Select Page 0 w 30 00 00 # # Power up LADC/RADC w 30 51 c0 # # Unmute LADC/RADC w 30 52 00 # ###############################################
Regards.