Hi,
I'm having issues using DIX9211 Ti device and in particular receiving SPID signal.
I'm attaching here the waveform of the input signal acquired on the pin 37 RXIN0 (SPDIF at 48KHz). Then the schematic too.
This is the dump of Dix9211 registers at the boot:
00000020 00 00 01 04 00 01 01 00 03 0C FF FF 00 00 00 04
00000030 10 1A 22 22 C2 02 02 00 00 80 00 00 00 00
00000040 C0 FF 02
00000050 00 00 00 00 00 00
00000060 44 10 00 00 00 00 00 00 00 00 00 00 00 00 0F 40
00000070 00 00 00 00 00 00 00 00 3D 00 00 00 00 F0 0F
This instead the register dump after the initialization:
00000020 00 00 01 04 00 01 01 00 03 0C 00 00 00 00 00 04
00000030 10 1A 22 22 C0 00 00 01 19 80 00 00 00 00
00000040 C0 FF 02
00000050 00 00 00 00 00 00
00000060 44 10 00 00 00 00 00 00 00 00 00 00 00 00 0F 40
00000070 00 00 00 00 00 00 00 00 3D 00 00 00 00 F0 0F
Can you help to understand the issue?
I think there could be some register to be properly initialized before I receive SPID on Channel0 at 48KHz.
Thanks a lot.
Best regards Edo