This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3204: AGC Target Level runtime modification

Part Number: TLV320AIC3204

Hi,

Can I change AGC Target Level value runtime for TLV320AIC3204? Specifically Right channel AGC control register D6-D4. The registers are getting modified runtime and I have verified that the changes take place but I don't see its effect in resultant audio when I set 6= -20dB, 4= -14dB, 2 = -10dB. The input audio is 1KHz sine wave tone. Also See the attached snap of audio which is not changing according to Target level changed at runtime.

Thanks,

Kishan