This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC33: Need some clarifications about the TLV320AIC33IRGZR audio codec

Part Number: TLV320AIC33

Hai,

    We are using  TLV320AIC33IRGZR audio codec with IMX8 M PLUS PROCESSOR. In that audio codec, I have a few queries.

1. I am using audio input with two-lane (LANE2_LP & LANE2_RP) remaining LANE2_LM & LANE2_RM should be tied with 0.47uF and 1K resistor to the analog ground ?? is it correct ?

2. This audio codec has a thermal pad, In the datasheet not mentioned thermal should tie with the ground? can I connect to the ground or floating?

3. In this audio codec driver will be supported IMX8 m plus processor

Thanks

Pandian