Hi, I am trying to upgrade audio preamplifiers which currently use a single IC -TL071. I have identified an IC -LT1115 which appears to have an ultra low noise level and a very high gain. This is supported by Spice circuit analysis, but Spice does not offer such good analysis software as TINA. Can you help me to transfer the LT1115 Macro from Spice to TINA?
Alternatively can you suggest a Texas IC with a noise of less than 1nV/(square root of Hz) and a gain of >100dB, for a frequency range of 1kHz to 40kHz. The IC needs to be equivalent to a TL071 in terms of pin-out and hopefully would be an 8 leg pin type (ie a PDIP-8) which can be soldered into the existing pcbs. The other requirement is I would need to analyse the IC's performance on TINA so a macro would be essential.
Thanking you in advance.
Allan