We are developing a TLV320AIC3254 connected to a CC2654. This application uses BLE to pair with two remote mics. We would like to connect the CC2652 to the AIC3254 with an I2C and two I2S connections. The audio signals are inputs to the AIC3254. We would like to send the audio as close to simultaneous as possible and have the codec mesh the signals. Is this possible?
The application guide says that only one I2S may be active a time. In addition, it appears that the secondary options for WCLK are output only. So, is possible to configure the AIC3254 to have two I2S inputs at all?
Our use case may be able to tolerate switching between the two I2S inputs. Assuming that input switching is acceptable to our customers, would this be accomplished through Page 0, Register 33?
Thank you for your input.