This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LME49600: Open Loop Distortion and Pspice Model

Part Number: LME49600

To Whom It May Concern,

In the data sheet the distortion performance is specified with an LME49710 in circuit which I assume is used to linearize the LME49600. I simulated the LME49600 using Pspice and it shows the highest harmonic level at about -140dBc with a 20Vpp sinewave output driving a 50 ohm load. Does the Pspice model include the LME49710 or is the LME49600 distortion not modeled? 

Thanks,

Shawn