Two questions
1.What is the function of the input signal mic1lp transmitted to the DAC in the figure below?
2. If I only use sound input and speaker, can I only connect MIC1LP, MIC1LM,I2S interface,SPKP,SPKM. Connect the interface in the figure below。The interface in the red box is not used