This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3254: ADC Powered Down when AGC is enabled

Part Number: TLV320AIC3254

Hi

While using the AGC function, we encountered the ADC power down issue.

We try to check/monitor the power up status of the ADC(read Page 0 / Register 36 (ADC Flag Register) ).

The input source is the some pop music, when we try to increase the volume of input source, the ADC Power Status Flag become to 0, when we decrease the volume of input source, the ADC Power Status Flag become to 1. Do you have any suggestions for us?

BR

Trevor