Part Number: PCM1807
Hello,
I am modifying an old design where a DSP generated a MCLK for the slave devices from an oscillator (12.288MHz). I have changed the DSP and the new one cannot output a MCLK, so I am stuck at this point. I am working at 48kHz of f_s and a relationship of 256 between BCLK and LRCLK.
I have 2 questions here:
- Can I use the same oscillator (ABRACON ASFL1-12.288MHz-LR) for various components? In my case I do need it for the DSP and this chip, at least, and then I am using a second ADC (PCM1895) where it can work with an internal PLL with the BCLK. So at least it would need to drive the DSP and this PCM1807, and the best case would be for the three chips. If this option is possible, what would I need? Just split the clock line near the oscillator output and add terminating resistors?
- If this option is not possible, I would like if the SCLK and the BCLK can be driven by the same signal, as they share the same frequency (48000 * 256 = 12.288MHz)
Thanks in advance!
Best regards,
Manuel