Hi ,
I am using PCM3168PAP in my design. I am using audio input signals in balanced mode.
1. Table 8.3 of datasheet shows Differential input signal rms value and single-ended input signal rms value. What is the difference between them.
2. Whether Analog Output Voltage =8Vpp same as differential output voltage swing.
3. What is Digital filter roll-off control. What is the use of the same.
4. What is the maximum rms analog input value that can be given to Audio Codec after which distortion can be observed in Audio output.
5. During my testing with Audio Codec, I am observing that distortion happens when turning audio input signal beyond 1.5V rms then goes away when turning the generator down to 1.5V RMS. What may be the reason for the same.