Other Parts Discussed in Thread: TAS5825M, PUREPATHCONSOLE,
Hey,
I am using:
PPC3 - v.3.21 Plattform: Build 306
TAS5825M: 3.1.12
with PurePathConsole Motherboard AIP006G
I am wondering that I only can select the TAS5825M (not the "TAS5825MEVM-SB" board):
After selection of audio feature/setup even the EVM layout looks different
with two TAS5825 amps, but TAS5825MEVM-SB has TAS5720 amp as second one.
The audio feature/setup loading is then successfull, but shortly after dialog closes, the I2C error appears:
Then EVM board is running, but I often get like "frozen states", where Amplifier is muting and only a full reset (with complete parameter writing) will help.
The System-Check is correct, except the HardwareID.