If I insert OMTP Headset in J4 will i be able to use use both speaker and mic of the headset? in other words, will i be able to talk and hear on headset?
Or should we use only headphone as mentioned in schematic?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If I insert OMTP Headset in J4 will i be able to use use both speaker and mic of the headset? in other words, will i be able to talk and hear on headset?
Or should we use only headphone as mentioned in schematic?
Hi Nikhil,
Today is a TI Holiday and our experts are out of office. Please give us another day to look at and answer your question. For record keeping purposes please do not reply to this message unless 48 hours have passed without a response.
Thank you for your patience,
Jeff
Hi,
The OMTP headset will fit in this audio jack as the GND pin is in the last sleeve, but the 3rd sleeve in the EVM is a MICDET which is for headset detection and not MIC input.
Regards.
Correct, but if i insert a jumper for W3 and W1(3-2), one should be able to Use both mic input (MIC1LP) and MICDETright?
On this question is yes, but on the previous question it is with headphone jack which does not connect to MIC.