Hello,
According to Absolute Maximum Ratings, it is described about SD pin as following.
"(2) The voltage slew rate of these pins must be restricted to no more than 10 V/ms. For higher slew rates, use a 100 kΩ resister in series
with the pins."
My customer is asking about the resister in series with SD pin..
(Question)
1) According to Typical Applications(Figure.18/19), 10 kΩ resister in series with SD pin is used.
In this case ,why is 100 kΩ resister not used? Could you please tell us reason?
2) Is resister value needed to change depending on slew rate of SD pin?
Regards,
Tao_2199