Other Parts Discussed in Thread: PUREPATHCONSOLE
Hi:
1.PUREPATHCONSOLE ,
2.Please help to give a version of the recommended register configuration for the following usage conditions.
45W*4ch@2Ω;PWM:2.1MHz;STBY :2mode
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
1.PUREPATHCONSOLE ,
2.Please help to give a version of the recommended register configuration for the following usage conditions.
45W*4ch@2Ω;PWM:2.1MHz;STBY :2mode
Hi,
You can refer below script.
note: w is write action; r is read action; 5A is device address;
w 5A 30 80 # clear fault
w 5A 01 80 # reset
w 5A 03 AA #22dB Gain
w 5A 36 20 #slew rate 20:1.2V, 30:0.8V, 00:2.8V, 10:2.0V, 23 for 384KHz.
w 5A 37 22 #22:default dwell, FB/FC/FD fractional,
w 5A 38 A0 #bit7:enable SS, bit5:4 SS depth, bit3:0 step
w 5A 39 40 #180deg
w 5A 3A 62
w 5A 04 00 # set play
r 5A 00 40 # read registers