Other Parts Discussed in Thread: TAS5825MEVM,
Hello:
Can TAS5828M be controlled with the TAS5825MEVM control board? In addition, why is there no Stereo2.1 application in TAS5828M for PPC3? Is TAS5828M not supported?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello:
Can TAS5828M be controlled with the TAS5825MEVM control board? In addition, why is there no Stereo2.1 application in TAS5828M for PPC3? Is TAS5828M not supported?
Hi Huiquan
The register address in TAS5828 is different with TAS5825. I'm afraid you can't get the correct results using TAS5825 PPC3 to control TAS5828.
TAS5828 can support Stero2.1 mode, only our software team haven't found the bandwidth to build this function into PPC3. May I know what is the system level topology we are going to use? If we are planning using two piece of TAS5828, we suggest to use one as Stero 2.0 mode, and another use Mono 1.0 mode.
Again, I want to use one device to drive the treble and midpitch(Mono), and the other device to drive the bass. Can TAS5828M support it? How to do that?Thanks!