Other Parts Discussed in Thread: TAS2560
I would like to use the TAS2560EVM to send I2S data to the TAS2560 at a different sample rate. Is it possible? I believe the default rate it is sending to the TAS2560 is 48 kHz.
In our custom application, we would be sending 16 kHz sample rate audio. Can I test this using the EVM?
Additionally, what are the correct settings for sending audio only via BCLK (MCLK left floating) at 16kHz?
Using the Create Dump File, the output seems incorrect:
During testing, I had to set register 0x0F to 0x00 to get audio via BCLK. However the audio is degraded and sounds more muffled with high gain noise, as if someone turned up to max volume, but voice portion was only half way.
I noticed changing setting PLL ICTRL to 1 helped, but I don't see documentation on what that register does (in the datasheet):
Thank you for your help.