Other Parts Discussed in Thread: TAS5825M
Hello,
I am using the PPC3 interface and motherboard along with the TAS5825MEVM and I am trying to connect to my Prototype PCBA's. The I2C address of the TAS5825M on my PCBA is set to 9C. I have made connections to the I2C bus and the I2S bus. I am having difficulty getting the system to pass audio from the PPC3 to my board. I had it working at one point but soon after I was no longer able to make it work. I have 5 boards to be tested. The first 4 seemed to connect and pass audio just fine but when I tested the 5th board I was not able to get it to work. Assuming that the last board may be bad, I attempted to re-test one of the first 4 that had already worked and now I can't get any of the 5 boards to connect and pass audio. Nothing has changed that I am aware of in the configuration or setup during this process. I would appreciate any help in troubleshooting this problem.
Best regards, Jim Albert