This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6205A1: TPA6205A and TPA6204A/TPA6211A Input impedance's

Part Number: TPA6205A1
Other Parts Discussed in Thread: TPA6204A1, , TPA6211A1

Comparing the datasheets for the TPA6205A  and TPA6204A/TPA6211A Input impedance's, I see and input impedance of 2Mohm for the TPA6205A and an input impedance of 40Kohm (typ.) for the TPA6211A and no input impedance for TPA6204A.   Could I assume if each has the same Rf of 40Kohm 1% with the TPA6205A Rf being external at 40Kohm 1%, that the input impedance's are 40Kohm (nominal)?

I am more of a digital designer than analog and using the monolithic amplifier, I can integrate it easier into my design.