Other Parts Discussed in Thread: TAS5825M, TAS5828M,
I have written a driver for the TAS5825m that also works for the TAS5805m and the TAS5828m, based on work from Andy Liu and Daniel Beer. It uses DIG_VOL_CTL in Book 0x00 Page 0x00 Addr 0x4c for volume control without problems. Tested successfully on the Raspberri Pi Zero 2W with these devices. A firmware for configuring the DSP can be used, but is not necessary. A preliminary version is here:
// SPDX-License-Identifier: GPL-2.0 // // Driver for the TAS5805M Audio Amplifier // // Author: Andy Liu <andy-liu@ti.com> // Author: Daniel Beer <daniel.beer@igorinstitute.com> // Author: J.P. van Coolwijk <jpvc36@gmail.com> // // This is based on a driver originally written by Andy Liu at TI and // posted here: // // https://e2e.ti.com/support/audio-group/audio/f/audio-forum/722027/linux-tas5825m-linux-drivers // // It has been simplified a little and reworked for the 5.x ALSA SoC API. // Silicon available to me has a functional REG_VOL_CTL (0x4c), so the original dsp workaround is not necessary. // This driver works with a binary firmware file. When missing or invalid a minimal config for PVDD=24V is used. #include <linux/module.h> #include <linux/moduleparam.h> #include <linux/kernel.h> #include <linux/firmware.h> #include <linux/slab.h> #include <linux/of.h> #include <linux/init.h> #include <linux/i2c.h> #include <linux/regmap.h> #include <linux/gpio/consumer.h> #include <linux/regulator/consumer.h> #include <linux/atomic.h> #include <linux/workqueue.h> #include <sound/soc.h> #include <sound/pcm.h> #include <sound/initval.h> #include <sound/tlv.h> // New /* Datasheet-defined registers on page 0, book 0 */ #define REG_PAGE 0x00 #define REG_DEVICE_CTRL_1 0x02 #define REG_DEVICE_CTRL_2 0x03 #define REG_SIG_CH_CTRL 0x28 #define REG_SAP_CTRL_1 0x33 #define REG_FS_MON 0x37 #define REG_BCK_MON 0x38 #define REG_CLKDET_STATUS 0x39 #define REG_VOL_CTL 0x4c #define REG_AGAIN 0x54 #define REG_ADR_PIN_CTRL 0x60 #define REG_ADR_PIN_CONFIG 0x61 #define REG_CHAN_FAULT 0x70 #define REG_GLOBAL_FAULT1 0x71 #define REG_GLOBAL_FAULT2 0x72 #define REG_FAULT 0x78 #define REG_BOOK 0x7f #define TAS5805M_RATES (SNDRV_PCM_RATE_8000_96000) #define TAS5805M_FORMATS (SNDRV_PCM_FMTBIT_S16_LE | SNDRV_PCM_FMTBIT_S20_3LE |\ SNDRV_PCM_FMTBIT_S24_LE | SNDRV_PCM_FMTBIT_S32_LE) /* DEVICE_CTRL_2 register values */ #define DCTRL2_MODE_DEEP_SLEEP 0x00 #define DCTRL2_MODE_SLEEP 0x01 #define DCTRL2_MODE_HIZ 0x02 #define DCTRL2_MODE_PLAY 0x03 #define DCTRL2_MUTE 0x08 #define DCTRL2_DIS_DSP 0x10 /* REG_FAULT register values */ #define ANALOG_FAULT_CLEAR 0x80 /* This sequence of register writes must always be sent, prior to the * 5ms delay while we wait for the DSP to boot. * Sending 0x11 to DCTL2 resets the volume setting, so we send 0x01. */ static const uint8_t dsp_cfg_preboot[] = { 0x00, 0x00, 0x7f, 0x00, 0x03, 0x02, 0x01, 0x10, // reset dsp & write DCTRL2_MODE_HIZ to DCTL2, keeps TLDV setting 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x7f, 0x00, 0x03, 0x02, }; static const uint8_t dsp_cfg_firmware_missing[] = { 0x00, 0x00, 0x7f, 0x00, 0x54, 0x03, 0x78, 0x80, // minimal config for PVDD = 24V when firmware is missing }; struct tas5805m_priv { struct regulator *pvdd; struct gpio_desc *gpio_pdn_n; uint8_t *dsp_cfg_data; int dsp_cfg_len; struct regmap *regmap; bool is_powered; bool is_muted; }; static void tas5805m_refresh(struct snd_soc_component *component) { struct tas5805m_priv *tas5805m = snd_soc_component_get_drvdata(component); struct regmap *rm = tas5805m->regmap; regmap_write(rm, REG_PAGE, 0x00); regmap_write(rm, REG_BOOK, 0x00); regmap_write(rm, REG_PAGE, 0x00); /* Set/clear digital soft-mute */ regmap_write(rm, REG_DEVICE_CTRL_2, (tas5805m->is_muted ? DCTRL2_MUTE : 0) | DCTRL2_MODE_PLAY); regmap_write(rm, REG_FAULT, ANALOG_FAULT_CLEAR); // Is necessary for compatibility with TAS5828m } static const SNDRV_CTL_TLVD_DECLARE_DB_SCALE(tas5805m_vol_tlv, -10350, 50, 1); // New (name, min, step, mute) static const struct snd_kcontrol_new tas5805m_snd_controls[] = { // New SOC_SINGLE_TLV ("Master Playback Volume", REG_VOL_CTL, 0, 255, 1, tas5805m_vol_tlv), // (xname, reg, shift, max, invert, tlv_array) }; static void send_cfg(struct regmap *rm, const uint8_t *s, unsigned int len) { unsigned int i; for (i = 0; i + 1 < len; i += 2) regmap_write(rm, s[i], s[i + 1]); } /* The TAS5805M DSP can't be configured until the I2S clock has been * present and stable for 5ms, or else it won't boot and we get no * sound. */ static int tas5805m_trigger(struct snd_pcm_substream *substream, int cmd, struct snd_soc_dai *dai) { struct snd_soc_component *component = dai->component; struct tas5805m_priv *tas5805m = snd_soc_component_get_drvdata(component); struct regmap *rm = tas5805m->regmap; unsigned int chan, global1, global2; switch (cmd) { case SNDRV_PCM_TRIGGER_START: // 1 case SNDRV_PCM_TRIGGER_RESUME: // 6 case SNDRV_PCM_TRIGGER_PAUSE_RELEASE: // 4 dev_dbg(component->dev, "DSP startup\n"); /* We mustn't issue any I2C transactions until the I2S * clock is stable. Furthermore, we must allow a 5ms * delay after the first set of register writes to * allow the DSP to boot before configuring it. */ usleep_range(5000, 10000); send_cfg(rm, dsp_cfg_preboot, // reset all / dsp regs & write DCTRL2_MODE_HIZ to DCTL2 ARRAY_SIZE(dsp_cfg_preboot)); // 0x01 0x11 kills TLVD volume setting usleep_range(5000, 15000); if(tas5805m->dsp_cfg_data){ send_cfg(rm, tas5805m->dsp_cfg_data, // write firmware tas5805m->dsp_cfg_len); } else { send_cfg(rm, dsp_cfg_firmware_missing, // write minimal config ARRAY_SIZE(dsp_cfg_firmware_missing)); } tas5805m->is_powered = true; tas5805m_refresh(component); break; case SNDRV_PCM_TRIGGER_STOP: // 0 case SNDRV_PCM_TRIGGER_SUSPEND: // 5 case SNDRV_PCM_TRIGGER_PAUSE_PUSH: // 3 dev_dbg(component->dev, "DSP shutdown\n"); tas5805m->is_powered = false; regmap_write(rm, REG_PAGE, 0x00); // rm, 0x00, 0x00 regmap_write(rm, REG_BOOK, 0x00); // rm, 0x7f, 0x00 regmap_read(rm, REG_CHAN_FAULT, &chan); // rm, 0x70, 0x00 regmap_read(rm, REG_GLOBAL_FAULT1, &global1); // rm, 0x71, 0x00 regmap_read(rm, REG_GLOBAL_FAULT2, &global2); // rm, 0x72, 0x00 dev_dbg(component->dev, "fault regs: CHAN=%02x, GLOBAL1=%02x, GLOBAL2=%02x\n", chan, global1, global2); regmap_write(rm, REG_DEVICE_CTRL_2, // ramp volume up / down DCTRL2_MODE_PLAY | DCTRL2_MUTE); // rm, 0x03, 0x0b break; default: return -EINVAL; } return 0; } static const struct snd_soc_dapm_route tas5805m_audio_map[] = { { "DAC", NULL, "DAC IN" }, { "OUT", NULL, "DAC" }, }; static const struct snd_soc_dapm_widget tas5805m_dapm_widgets[] = { SND_SOC_DAPM_AIF_IN("DAC IN", "Playback", 0, SND_SOC_NOPM, 0, 0), SND_SOC_DAPM_DAC("DAC", NULL, SND_SOC_NOPM, 0, 0), SND_SOC_DAPM_OUTPUT("OUT") }; static const struct snd_soc_component_driver soc_codec_dev_tas5805m = { .controls = tas5805m_snd_controls, .num_controls = ARRAY_SIZE(tas5805m_snd_controls), .dapm_widgets = tas5805m_dapm_widgets, .num_dapm_widgets = ARRAY_SIZE(tas5805m_dapm_widgets), .dapm_routes = tas5805m_audio_map, .num_dapm_routes = ARRAY_SIZE(tas5805m_audio_map), .use_pmdown_time = 1, .endianness = 1, }; static int tas5805m_mute(struct snd_soc_dai *dai, int mute, int direction) { struct snd_soc_component *component = dai->component; struct tas5805m_priv *tas5805m = snd_soc_component_get_drvdata(component); dev_dbg(component->dev, "set mute=%d (is_powered=%d)\n", mute, tas5805m->is_powered); tas5805m->is_muted = mute; if (tas5805m->is_powered) tas5805m_refresh(component); return 0; } static const struct snd_soc_dai_ops tas5805m_dai_ops = { .trigger = tas5805m_trigger, .mute_stream = tas5805m_mute, .no_capture_mute = 1, }; static struct snd_soc_dai_driver tas5805m_dai = { .name = "tas5805m-amplifier", .playback = { .stream_name = "Playback", .channels_min = 2, .channels_max = 2, .rates = TAS5805M_RATES, .formats = TAS5805M_FORMATS, }, .ops = &tas5805m_dai_ops, }; static const struct regmap_config tas5805m_regmap = { .reg_bits = 8, .val_bits = 8, /* We have quite a lot of multi-level bank switching and a * relatively small number of register writes between bank * switches. */ .cache_type = REGCACHE_NONE, }; static int tas5805m_i2c_probe(struct i2c_client *i2c) { struct device *dev = &i2c->dev; struct regmap *regmap; struct tas5805m_priv *tas5805m; char filename[128]; const char *config_name; const struct firmware *fw; int ret; regmap = devm_regmap_init_i2c(i2c, &tas5805m_regmap); if (IS_ERR(regmap)) { ret = PTR_ERR(regmap); dev_err(dev, "unable to allocate register map: %d\n", ret); return ret; } tas5805m = devm_kzalloc(dev, sizeof(struct tas5805m_priv), GFP_KERNEL); if (!tas5805m) return -ENOMEM; tas5805m->pvdd = devm_regulator_get(dev, "pvdd"); if (IS_ERR(tas5805m->pvdd)) { dev_err(dev, "failed to get pvdd supply: %ld\n", PTR_ERR(tas5805m->pvdd)); return PTR_ERR(tas5805m->pvdd); } dev_set_drvdata(dev, tas5805m); tas5805m->regmap = regmap; tas5805m->gpio_pdn_n = devm_gpiod_get(dev, "pdn", GPIOD_OUT_LOW); if (IS_ERR(tas5805m->gpio_pdn_n)) { dev_err(dev, "error requesting PDN gpio: %ld\n", PTR_ERR(tas5805m->gpio_pdn_n)); return PTR_ERR(tas5805m->gpio_pdn_n); } /* This configuration must be generated by PPC3. The file loaded * consists of a sequence of register writes, where bytes at * even indices are register addresses and those at odd indices * are register values. * * The fixed portion of PPC3's output prior to the 5ms delay * should be omitted. */ if (device_property_read_string(dev, "ti,dsp-config-name", &config_name)) config_name = "default"; snprintf(filename, sizeof(filename), "tas5805m_dsp_%s.bin", config_name); ret = request_firmware(&fw, filename, dev); if (ret) { dev_err(dev, "firmware not found, using minimal config\n"); goto err; } if ((fw->size < 2) || (fw->size & 1)) { dev_err(dev, "firmware is invalid, using minimal config\n"); release_firmware(fw); goto err; } tas5805m->dsp_cfg_len = fw->size; tas5805m->dsp_cfg_data = devm_kmalloc(dev, fw->size, GFP_KERNEL); if (!tas5805m->dsp_cfg_data) { dev_err(dev, "firmware is not loaded, using minimal config\n"); release_firmware(fw); goto err; } memcpy(tas5805m->dsp_cfg_data, fw->data, fw->size); release_firmware(fw); err: /* Do the first part of the power-on here, while we can expect * the I2S interface to be quiet. We must raise PDN# and then * wait 5ms before any I2S clock is sent, or else the internal * regulator apparently won't come on. * * Also, we must keep the device in power down for 100ms or so * after PVDD is applied, or else the ADR pin is sampled * incorrectly and the device comes up with an unpredictable I2C * address. */ ret = regulator_enable(tas5805m->pvdd); if (ret < 0) { dev_err(dev, "failed to enable pvdd: %d\n", ret); return ret; } usleep_range(100000, 150000); gpiod_set_value(tas5805m->gpio_pdn_n, 1); usleep_range(10000, 15000); /* Don't register through devm. We need to be able to unregister * the component prior to deasserting PDN# */ ret = snd_soc_register_component(dev, &soc_codec_dev_tas5805m, &tas5805m_dai, 1); if (ret < 0) { dev_err(dev, "unable to register codec: %d\n", ret); gpiod_set_value(tas5805m->gpio_pdn_n, 0); regulator_disable(tas5805m->pvdd); return ret; } return 0; } //static void tas5805m_i2c_remove(struct i2c_client *i2c) // for linux-6.xx static int tas5805m_i2c_remove(struct i2c_client *i2c) // for linux-5.xx { struct device *dev = &i2c->dev; struct tas5805m_priv *tas5805m = dev_get_drvdata(dev); snd_soc_unregister_component(dev); gpiod_set_value(tas5805m->gpio_pdn_n, 0); usleep_range(10000, 15000); regulator_disable(tas5805m->pvdd); // for linux-6.xx return 0; // for linux-5.xx } static const struct i2c_device_id tas5805m_i2c_id[] = { { "tas5805m", }, { } }; MODULE_DEVICE_TABLE(i2c, tas5805m_i2c_id); #if IS_ENABLED(CONFIG_OF) static const struct of_device_id tas5805m_of_match[] = { { .compatible = "ti,tas5805m", }, { } }; MODULE_DEVICE_TABLE(of, tas5805m_of_match); #endif static struct i2c_driver tas5805m_i2c_driver = { .probe_new = tas5805m_i2c_probe, .remove = tas5805m_i2c_remove, .id_table = tas5805m_i2c_id, .driver = { .name = "tas5805m", .of_match_table = of_match_ptr(tas5805m_of_match), }, }; module_i2c_driver(tas5805m_i2c_driver); MODULE_AUTHOR("Andy Liu <andy-liu@ti.com>"); MODULE_AUTHOR("Daniel Beer <daniel.beer@igorinstitute.com>"); MODULE_AUTHOR("J.P. van Coolwijk <jpvc36@gmail.com>"); MODULE_DESCRIPTION("TAS5805M Audio Amplifier Driver"); MODULE_LICENSE("GPL v2");
Device tree overlay for Rpi:
// Definitions for AmpliMuse Amp // dtc -I dts -O dtb -o /boot/overlays/tas58xx.dtbo tas58xx-overlay.dts // bash: "sudo dtoverlay tas58xx <i2creg=...> <firmware=...>" // /boot/config.txt: "dtoverlay=tas58xx<,i2creg=...><,firmware=...>" // i2creg: TAS5805M@0x2c, TAS5806M@0x2c, TAS5822M@0x2c, TAS5825M@0x4c, TAS5825P@0x4c, TAS5828M@0x60 /dts-v1/; /plugin/; / { compatible = "brcm,bcm2835"; fragment@0 { target = <&i2s>; __overlay__ { status = "okay"; }; }; fragment@1 { target = <&i2c1>; __overlay__ { status = "okay"; clock-frequency = <400000>; #address-cells = <1>; #size-cells = <0>; codec: tas58xx@reg { #sound-dai-cells = <0>; compatible = "ti,tas58xx"; reg = <0x2c>; // pvdd-supply = <&audiopwr>; pvdd-supply = <&vdd_3v3_reg>; pdn-gpios = <&gpio 4 0>; ti,dsp-config-name = "default"; }; }; }; fragment@2 { target = <&sound>; __overlay__ { status = "okay"; compatible = "simple-audio-card"; label = "AmpliMuse"; simple-audio-card,dai-link { /* DAC */ format = "i2s"; bitclock-master = <&dailink_master>; frame-master = <&dailink_master>; dailink_master: cpu { sound-dai = <&i2s>; dai-tdm-slot-num = <2>; dai-tdm-slot-width = <32>; }; codec { sound-dai = <&codec>; }; }; }; }; __overrides__ { firmware = <&codec>,"ti,dsp-config-name"; i2creg = <&codec>,"reg:<>"; }; };
I am working to get this driver submitted to the mainline Linux distribution. Before doing so I need to know the following: What is the reason that in the original driver on: https://e2e.ti.com/support/audio-group/audio/f/audio-forum/722027/linux-tas5825m-linux-drivers a bypass via Book 0x8c Page 0x2a Addr 0x24 and 0x28 is used?