Dear Sir,
In TAS3208 Datasheet page 1 it mention TAS3208 I2S slave mode is 44.1KHz and 48KHz only master mode is 48KHz only but in TI website
http://focus.ti.com/docs/prod/folders/print/tas3208.html Parameter table it mention Fs 32 to 48KHz, and in datasheet p18 mention sample rate support 32K / 44.1K /48K, I want ot confirm TAS3208 I2S input support 32K sample rate?
In datasheet page 10. it is mentioned
In slave mode, all incoming serial audio data must be synchronous to an incoming
LRCLKIN of 32, 44.1, or 48 kHz. The TAS3208 does not support the use of an external
(i.e., 24-MHz) clock input into XTALI.
That means TAS3208 digital audio input 32 /44.1 /48KHz for LRCLK input
BR
Edwin