Hi,
We're using the TLV320ADC6140 to sample signal from a microphone which it's lowest voltage level is -111dBV (5.6µVRMS) . The mic connected differentially to the ADC.
The ADC is fed with 3V and VREF is set to default, i.e. Differential Full Scale Input supported = 2 VRMS.
Now,
- What is the ENOB of the ADC? Or, what is the lowest voltage level that can be sampled with the TLV320ADC6140 ?
- What should be the internal amplifier gain while we want to be able to sample -111dBV signals? Do we need external amplifier?
Please advise,