Hi
there is a project active 2.0 speaker , using TAS5805M as amplifier.
2pcs TAS5805M in PBTL with 4Ω,but when playing music, it is easy to music off, specially in bass music.
If using sine wave and resistive load, it is not easy to make music off.
when music without resistive load, it will be 100% to make music off.
Chip temperature is high, the music is not easy to off.
We also tested when not connecting TAS5805M 4 outputs, the music will be easy off in any mode.
0x70 shows ch1 or ch2 over current.
coukd you please tell us the chip protect reason and how to solve it?
thank you