This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3250: TPA3250 power output

Part Number: TPA3250

Hi we are using TPA3250 in PBTL mode

using this for audio power amplifier (woofer low frequency application)

running at 35VDC, 

Query is when we are running at 100 hz input signal ,,,out put is coming 100W only at 1% THD clean sine wave.

we are looking for 125W, 1% THD, clean sine wave..how to achieve this.

pl suggest

rgds