Hello again,
a stereo amplifier consumes at PVDD = 12V in play mode, when no input signal is present, about 1W power, which is quite a lot.(so 0.5W idle power per speaker) After some time the magnets of the speakers heat up to about 30°. The voice coil is then probably even hotter. How can I reduce this idle current? Why do the loudspeakers get warm? Shouldn't almost no current flow through the speakers when no signal is played?
Modulation frequency: 782kHz
Loop BW: 175kHz
Modulation scheme: BD
Output filter: ferrite bead (NFZ2MSM301SN10L)
PVDD: 12V
Loudspeaker: 3.7 Ohm; 0.07mH