Other Parts Discussed in Thread: TAS2780
Team, we're designing an amplifier in a digital carrier board hosting Jetson GPU. The GPU offers an I2S interface for audio playback, and we prefer to choose the TAS2770 20-W as the amplifier. The speaker would be 8Ohm / 15W RMS / 23 W Max. The amplifier IC will be powered from the carrier card with a 12V, 2A source. The amplifier/sound usually does not demand continuous operation for more than 1 minute, as the purpose is to give quick audio alerts. We're in the early stages of the feasibility check and would like to see if there are better alternatives from TI as well.