This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM386: Interface with 8ohm 1W speeker

Part Number: LM386


Hello,

I am designing speaker driving amplifier circuit that circuit uses LM386N-4.
Section 6.5 on data sheet shows output power characteristic for LM386N-4.
The conditions of this output power characteristic are Vs=16V and RL=32ohm.

I will connect 8ohm 1W speaker for this amplifier circuit and supplying +15V to LM386N-4.
I would like to check if there is any problem when connecting an 8Ω, 1W speaker to this circuit.

Regards,

MESH