This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3105EVM-K: Bill of Materials (BOM) is incorrect

Part Number: TLV320AIC3105EVM-K
Other Parts Discussed in Thread: TLV320AIC3104

Hello, 

i want to point out that on this reference document the BOM does not match the schematic. 

  • SLAU217A–July 2007–Revised January 2014 TLV320AIC3105EVM and TLV320AIC3105EVM-PDK

Specifically the output capacitors on the LOP, LOM, etc lines C33-C36) don't match the BOM as the C33 is a 47uF 6.3V Ceramic Chip Capacitor, ±20%, X5R. and then C34 is a 0.1uF 16V Ceramic Chip Capacitor, ±10%, X7R. 

I think there are other errors too. I'm pretty sure that the correct value for each of these schematic items is 47uF 6.3V Ceramic Chip Capacitor, ±20%, X5R.