I would like to ask about the following three things about "BQ Structure (the graphical one on the left side of the GUI)" and "128 Tap FIR Filter" in the Equalizer/FIR Filter GUI.
・Are these differences only in operability?
・If I want to filter the input signal, can I use only one of them?
・When using these two filters, in what situations are they suitable?
I apologize for the many questions, but please answer them.
Takeru