Hello,
I am trying to generate microcontroller code using PPC3, but I cannot find the End-System Integration Page mentioned in the software manual to do so.
Is this feature available for the TAS6584-Q1?
Best regards,
Fernando C
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am trying to generate microcontroller code using PPC3, but I cannot find the End-System Integration Page mentioned in the software manual to do so.
Is this feature available for the TAS6584-Q1?
Best regards,
Fernando C
Hi Shadow,
I can do that.
Does TI have example scripts available for bringing up the amp in I2S mode?
Best regards,
Fernando C
Hi Fernando
The default register settings is I2S mode, 24bit word length. Only set the channel into PLAY would work normally.
Example you could use as below:
w c0 00 00
w c0 7f 00 # Go to Book0 Page0
w c0 01 18 # Reset device
w c0 02 01 # Use 1SPW, BTL
w c0 23 0A # default, word length 24bit
w c0 21 00 # default value, I2S mode
w c0 03 44 # Channel 1,2 PLAY
w c0 04 44 # Channel 3,4 PLAY