Other Parts Discussed in Thread: TAS2781
Dear sirs,
I'm using the TAS2781 EVM, there is a question about ultrasound mode. (PWR_MODE3)
The frequency reponse of 20Hz ~ 40kHz with PWR_MODE3, Fs = 96k, show as below (Which is capture from TAS2781 Datasheet)
But I measure TAS2781 EVM with APx525 + AUX0025 as the same condition in datasheet, I can not get the same result as above , please check the picture my measurement as below.
The frequency response in 20kHz ~ 40kHz seems something setting issue ?
PVDDH=18V, PVDDL=5V, Power=1W, Fs=96kHz
I'm using the PurePath Console direct I2C to settle up the TAS2781, the command what I use are getting from TAS2781 datasheet 10.5 Initial Device Configuration - PWR_MODE3
Is there anything else I need to configure for this mode?