Hi.
Can this device drive a 3ohm 3.7W speaker?
Please tell me PO at PBTL (mono),THD+N = 10%, f = 1 kHz, PVCC = 5 V, RL = 3 Ω.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
Can this device drive a 3ohm 3.7W speaker?
Please tell me PO at PBTL (mono),THD+N = 10%, f = 1 kHz, PVCC = 5 V, RL = 3 Ω.
Hi,
I do not have the data. Suggest you can apply one EVM board and do the evaluation.