This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A227E: Schematic check

Part Number: TS3A227E

Hi TI Teams,

Can u help to check the schematic of TS3A227E and give us some suggestion? The schematic is as below.

TS3A227E_Schematic.pdf

Also we still have some question for the using of TS3A227E,  see as below:

1) The TS3A227E put on the right motherboard, and Audio Jack on the left board, connected by the middle of the line. From the datasheet we can learned that this design does not meet the requirements of layout , so is it necessary to put TS3A227E near Audio Jack.

2) Is it feasible that TS3A227E does not connect the I2C? 

3) If the TS3A227E is connected to I2C, is there any driver for it? What functions does the driver, and is there any difference with no drive?

4) Is there an Auto Switch with Codec design? And how to use MIC-PRES? The Audio codec is Realtek ALC5640 and CPU platform is ROCKCHIP, runing system is Android 12. Does the TS3A227E and ALC5640 cooperate at the software level (firmware communication) or at the hardware level (GPIO connection)?

Thanks,

Kind Regards