Other Parts Discussed in Thread: PCM5101, PCM5142
Hi Team,
Can you please check the inquiry below?
Using PCM5142EVM-U, if you look at this schematic below, there is a signal called: WCLK and I read on the datasheet TAS1020B has the same sample rate that in Input. I'm using Audacity software where I send a sine of 10 [KHz] with a sample rate of 48 [KHZ] ( note: I'm not using ASIO4ALL). As you can see in this picture I can come to measure the signal.
On TP28 but unfortunately, the sample rate is ALWAYS the same as you can see.
always 44.1 [KHz] and by the way, I'm using CodecControl to control the EvalBoard with the code called: "PCM5101_USB Playback" I didn't modify the code.
Let me know if you need more information and thanks in advance.
Regards,
Marvin