Dear Team,
Below is the block diagram of my first design using an audio power amplifier.
The input to the audio power amplifier comes from an SC200 module by Quectel.
The output of the PA is connected to a speaker.
I have couple of questions:
- Will the PA I selected w be able to drive this 4 ohm speaker?
- What are the things to be considered when selecting the PA for driving a speaker?
- How much power will I get at the output?
- In digikey during PA selection I can see that, Max Output Power x Channels @ Load is "3W x 1 @ 4Ohm" May I know what you mean by this?
- What will happen if I used the PA with above spec to 8 ohm speaker
Below is my Schematic.Could you please review the same.
Regards
HARI