This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5825M: When increase volume over 75% TAS5825M will mute

Part Number: TAS5825M

Dear Sir

My TAS5825M application is 2.0 (Stereo BTL) System, when volume lower then 75% can normal play but if over 75% will mute.

I measure the GPIO 1 (mute)  when normal play the voltage is 1.5V and abnormal is 0.15V, i think the GPIO function not correct

How to check and setting GPIO function?

Below is .h file i built from PPC3 for reference.

5857.-3db_128.h

Thank you.

Knight.