Hi,
We are using TI CODEC part TLV320AIC3268IRGCT in our design. While CODEC validation we have seen that the ADC output count is less compared to actual input sinusoidal signal amplitude.
We are using a VOGAD IC prior to CODEC input so that a voltage of around 1Vpp to 1.2Vpp will be always available at CODEC ADC input. ADC input full scale range should support 0.5Vrms or 1.414Vpp.
If we are giving an input amplitude of 1Vpp ADC output is only around +-500 counts in amplitude which is significantly less than the input amplitude. We are getting +-500 counts with 0dB PGA gain at ADC front end. If we are increasing PGA gain to +6dB count is increasing. If PGA gain is increased to +12dB ADC count is reaching around +-2500 and is saturation. But ADC should saturate at full-scale range count of around +-32000.
Below is the CODEC register configuration for review.
Note: CODEC DAC is independently validated by output sinusoidal signal using FPGA DDS. We are facing issue with ADC performance.
Regards
Hafiz Haja