This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5122EVM-U: pop noise occur when power up, input I2S, exit or enter standby mode

Part Number: PCM5122EVM-U
Other Parts Discussed in Thread: PCM5122

Hi Team,

customer complain about PCM5122 pop noise. and I have replicate the pop noise on the EVM.

the PCM5122EVM have obvious pop noise when 3.3V power up, input I2S signal, exit or enter standby mode. please tell me how to avoid those pop noise.

1. on PCM5122EVM, connect the XSMT pin to ground maintain mute status, then power up the PCM5122 via the W4 +3.3V jumper, the pop noise occur. use the AP to record the pop noise as below.

2. still keep the XSMT pin connect to ground, input I2S into PCM5122,the pop occur as below AP record.

3 exit or enter the standby mode by the register 2, also have pop occur.

please help to fix above pop noise.

Thanks.

Anderson